SubdivisionProjectCageBuilderTypes Enumeration¶
NXOpen.Features.Subdivision.SubdivisionProjectCageBuilder.Types is an alias for NXOpen.Features.Subdivision.SubdivisionProjectCageBuilderTypes
-
class
NXOpen.Features.Subdivision.
SubdivisionProjectCageBuilderTypes
¶ Bases:
object
The type of projection
Enum Members
Enum Member Enum Member Description ToTarget Project on target ToAverage Project using best fit plane or axis AlignNormal Align edges normal to the specified plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-