SubdivisionPrimitiveShapeBuilderExSphereSubdivisionLevel Enumeration¶
NXOpen.Features.Subdivision.SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel is an alias for NXOpen.Features.Subdivision.SubdivisionPrimitiveShapeBuilderExSphereSubdivisionLevel
-
class
NXOpen.Features.Subdivision.
SubdivisionPrimitiveShapeBuilderExSphereSubdivisionLevel
¶ Bases:
object
Level of subdivisions of cubical cage to construct spherical primitive.
Enum Members
Enum Member Enum Member Description Base First Second -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-