SubdivisionLoftBuilder Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionLoftBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.SubdivisionLoftBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionLoftBuilder()
Default values.
Property Value CanSew 1 NumberOfSegments 1 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
CanSew | Returns or sets the value indicating if open edges of the loft mesh can be sewn with selected input open edges. |
Continuity | Returns or sets the continuity. |
IsClosed | Returns or sets the value indicating if the output mesh is closed. |
NumberOfSegments | Returns or sets the number of segments |
Sections | Returns the section objects for lofting |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivisionLoftBuilderContinuityType Enumeration | Type of continuity. |
Property Detail¶
CanSew¶
-
SubdivisionLoftBuilder.
CanSew
¶ Returns or sets the value indicating if open edges of the loft mesh can be sewn with selected input open edges.
-------------------------------------
Getter Method
Signature
CanSew
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanSew
Parameters: canSew (bool) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Continuity¶
-
SubdivisionLoftBuilder.
Continuity
¶ Returns or sets the continuity.
The continuity is used to specify creases in the limit surface corresponding to edges of the lofted region that are sewn with the primary existing region.
-------------------------------------
Getter Method
Signature
Continuity
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionLoftBuilderContinuityType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Continuity
Parameters: continuity ( NXOpen.Features.Subdivision.SubdivisionLoftBuilderContinuityType
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
IsClosed¶
-
SubdivisionLoftBuilder.
IsClosed
¶ Returns or sets the value indicating if the output mesh is closed.
-------------------------------------
Getter Method
Signature
IsClosed
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsClosed
Parameters: isClosed (bool) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
NumberOfSegments¶
-
SubdivisionLoftBuilder.
NumberOfSegments
¶ Returns or sets the number of segments
-------------------------------------
Getter Method
Signature
NumberOfSegments
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfSegments
Parameters: numberOfSegments (int) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Sections¶
-
SubdivisionLoftBuilder.
Sections
¶ Returns the section objects for lofting
-------------------------------------
Getter Method
Signature
Sections
Returns: Return type: NXOpen.Features.Subdivision.CageSectionDataList
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SubdivisionLoftBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.