SubdivisionExtrudeCageBuilderScalingMethodType Enumeration¶
NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilder.ScalingMethodType is an alias for NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderScalingMethodType
-
class
NXOpen.Features.Subdivision.
SubdivisionExtrudeCageBuilderScalingMethodType
¶ Bases:
object
Scaling method
Enum Members
Enum Member Enum Member Description Linear Scale in the specified direction Planar Scale in the plane normal to specified direction Uniform Scale uniformly all the directions -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-