SubdivisionExtrudeCageBuilderDirectionType Enumeration

NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilder.DirectionType is an alias for NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderDirectionType

class NXOpen.Features.Subdivision.SubdivisionExtrudeCageBuilderDirectionType

Bases: object

Represents the extrude direction.

Enum Members

Enum Member Enum Member Description
Inferred
Vector
Perpendicular
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.