SubdivisionConnectCageBuilderContinuityTypes Enumeration

NXOpen.Features.Subdivision.SubdivisionConnectCageBuilder.ContinuityTypes is an alias for NXOpen.Features.Subdivision.SubdivisionConnectCageBuilderContinuityTypes

class NXOpen.Features.Subdivision.SubdivisionConnectCageBuilderContinuityTypes

Bases: object

Represents the continuity type

Enum Members

Enum Member Enum Member Description
Smooth
Sharp
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.