SplitSubdivisionBodyBuilderInputBodyOptions Enumeration¶
NXOpen.Features.Subdivision.SplitSubdivisionBodyBuilder.InputBodyOptions is an alias for NXOpen.Features.Subdivision.SplitSubdivisionBodyBuilderInputBodyOptions
-
class
NXOpen.Features.Subdivision.
SplitSubdivisionBodyBuilderInputBodyOptions
¶ Bases:
object
Options indicating actions to be taken on input
Features.Subdivision.SubdivisionBody
featuresEnum Members
Enum Member Enum Member Description Keep Keep the feature as they are Hide Hide the features Delete Delete the features -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-