ImportSubdivisionGeometryBuilder Class¶
-
class
NXOpen.Features.Subdivision.
ImportSubdivisionGeometryBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.ImportSubdivisionGeometryBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateImportSubdivisionGeometryBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
CanCreateSingleFeature | Returns or sets the flag indicating if single feature should be created for all the disjoint regions of the subdivision geometry. |
FileName | Returns or sets the file name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CanCreateSingleFeature¶
-
ImportSubdivisionGeometryBuilder.
CanCreateSingleFeature
¶ Returns or sets the flag indicating if single feature should be created for all the disjoint regions of the subdivision geometry.
When false, separate feature will be created for each disjoint region.
-------------------------------------
Getter Method
Signature
CanCreateSingleFeature
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanCreateSingleFeature
Parameters: canCreateSingleFeature (bool) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
FileName¶
-
ImportSubdivisionGeometryBuilder.
FileName
¶ Returns or sets the file name.
Expects a file in standard ASCII Wavefront OBJ format used for base mesh definition of a subdivision geometry. Usage of OBJ files representing triangulated polygon mesh, similar to ones used for graphical rendering or higher resolution subdivision mesh is not recommended to be used. The solid model created from such mesh will have excessive amount of topology and the import operation will be inefficient.
-------------------------------------
Getter Method
Signature
FileName
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileName
Parameters: filename (str) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
Validate¶
-
ImportSubdivisionGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.