DefineWorkRegionBuilderFrozenRegionDefinitionMethods Enumeration¶
NXOpen.Features.Subdivision.DefineWorkRegionBuilder.FrozenRegionDefinitionMethods is an alias for NXOpen.Features.Subdivision.DefineWorkRegionBuilderFrozenRegionDefinitionMethods
-
class
NXOpen.Features.Subdivision.
DefineWorkRegionBuilderFrozenRegionDefinitionMethods
¶ Bases:
object
Method of defining frozen region.
Enum Members
Enum Member Enum Member Description Hidden Do not display the frozen region Colored Mark frozen region with color and do not allow its selection -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-