StyledCornerBuilderTrimAndSewMethodTypes Enumeration¶
NXOpen.Features.StyledCornerBuilder.TrimAndSewMethodTypes is an alias for NXOpen.Features.StyledCornerBuilderTrimAndSewMethodTypes
-
class
NXOpen.Features.
StyledCornerBuilderTrimAndSewMethodTypes
¶ Bases:
object
Trim and attach method types
Enum Members
Enum Member Enum Member Description NoTrim No trim TrimBlends Trim all blends TrimAll Trim blends and base wall TrimAndAttachBlends Trim and attach blends TrimAndAttachAll Trim and attach blends and base wall -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-