StyledCornerBuilderCurveControlTypes Enumeration¶
NXOpen.Features.StyledCornerBuilder.CurveControlTypes is an alias for NXOpen.Features.StyledCornerBuilderCurveControlTypes
-
class
NXOpen.Features.
StyledCornerBuilderCurveControlTypes
¶ Bases:
object
Curve control types
Enum Members
Enum Member Enum Member Description TopBaseCurve Use top curve BottomBridgeCurve Use bottom curve IsoCurveU Use iso u curve IsoCurveV Use iso v curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-