StyledBlendBuilderStyledBlendShapeControlType Enumeration¶
NXOpen.Features.StyledBlendBuilder.StyledBlendShapeControlType is an alias for NXOpen.Features.StyledBlendBuilderStyledBlendShapeControlType
-
class
NXOpen.Features.
StyledBlendBuilderStyledBlendShapeControlType
¶ Bases:
object
The shape control types
Enum Members
Enum Member Enum Member Description TangentCurve1 Tangent curve 1 TangentCurve2 Tangent curve 2 Depth Depth control Skew Skew control TangentMagnitude Tangent magnitude control -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-