StudioXformBuilderTranslationDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilder.TranslationDirectionType is an alias for NXOpen.Features.StudioXformBuilderTranslationDirectionType
-
class
NXOpen.Features.
StudioXformBuilderTranslationDirectionType
¶ Bases:
object
Represents the translation direction type
Enum Members
Enum Member Enum Member Description Xc Translate in X direction Yc Translate in Y direction Zc Translate in Z direction YcZc Translate on Y-Z plane XcZc Translate on X-Z plane XcYc Translate on X-Y plane ArbitraryDirection Translate in arbitrary direction ArbitraryPlane Translate on arbitrary plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-