StudioXformBuilderScalingDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilder.ScalingDirectionType is an alias for NXOpen.Features.StudioXformBuilderScalingDirectionType
-
class
NXOpen.Features.
StudioXformBuilderScalingDirectionType
¶ Bases:
object
Represents the scaling direction type
Enum Members
Enum Member Enum Member Description ScaleUniformly Scale uniformly PlaneOfCurve Scale on Plane of curve Xc Scale in X direction Yc Scale in Y direction Zc Scale in Z direction YcZc Scale on Y-Z plane XcZc Scale on X-Z plane XcYc Scale on X-Y plane ArbitraryDirection Scale in arbitrary direction ArbitraryPlane Scale on arbitrary plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-