StudioXformBuilderScalingCenterType Enumeration¶
NXOpen.Features.StudioXformBuilder.ScalingCenterType is an alias for NXOpen.Features.StudioXformBuilderScalingCenterType
-
class
NXOpen.Features.
StudioXformBuilderScalingCenterType
¶ Bases:
object
Represents the scaling center type
Enum Members
Enum Member Enum Member Description AboutObjectCenter Scale center at the object center AboutSelectedObject Scale center at the selected object AboutPoint Scale center at a point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-