StudioXformBuilderExScalingDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.ScalingDirectionType is an alias for NXOpen.Features.StudioXformBuilderExScalingDirectionType
-
class
NXOpen.Features.
StudioXformBuilderExScalingDirectionType
¶ Bases:
object
Represents the scaling direction type
Enum Members
Enum Member Enum Member Description WCS Scale in principal direction View Scale in view direction Vector Scale in vector direction Plane Scale in plane direction PlaneofCurve Scale on Plane of curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-