StudioXformBuilderExRotatingPivotType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.RotatingPivotType is an alias for NXOpen.Features.StudioXformBuilderExRotatingPivotType
-
class
NXOpen.Features.
StudioXformBuilderExRotatingPivotType
¶ Bases:
object
Represents the rotating pivot type
Enum Members
Enum Member Enum Member Description Rotateaboutobjectcenter Rotate pivot at the object center Rotateaboutselected Rotate pivot at the selected object Rotateaboutpoint Rotate pivot at a point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-