StudioXformBuilderExRotatingAxisType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.RotatingAxisType is an alias for NXOpen.Features.StudioXformBuilderExRotatingAxisType
-
class
NXOpen.Features.
StudioXformBuilderExRotatingAxisType
¶ Bases:
object
Represents the rotation axis type
Enum Members
Enum Member Enum Member Description WCS Rotate in principal direction View Rotate in view direction Vector Rotate in vector direction Plane Rotate on a plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-