StudioXformBuilderExPrincipalScalingDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.PrincipalScalingDirectionType is an alias for NXOpen.Features.StudioXformBuilderExPrincipalScalingDirectionType
-
class
NXOpen.Features.
StudioXformBuilderExPrincipalScalingDirectionType
¶ Bases:
object
Represents the principal scaling direction type
Enum Members
Enum Member Enum Member Description X Scale in X direction Y Scale in Y direction Z Scale in Z direction YZ Scale on Y-Z plane XZ Scale on X-Z plane XY Scale on X-Y plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-