StudioXformBuilderExPrincipalMovementDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.PrincipalMovementDirectionType is an alias for NXOpen.Features.StudioXformBuilderExPrincipalMovementDirectionType
-
class
NXOpen.Features.
StudioXformBuilderExPrincipalMovementDirectionType
¶ Bases:
object
Represents the principal movement direction type
Enum Members
Enum Member Enum Member Description X Translate in X direction Y Translate in Y direction Z Translate in Z direction YZ Translate on Y-Z plane XZ Translate on X-Z plane XY Translate on X-Y plane XYZ Translate on X-Y-Z coordinates -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-