StudioXformBuilderExMovementMethodType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.MovementMethodType is an alias for NXOpen.Features.StudioXformBuilderExMovementMethodType
-
class
NXOpen.Features.
StudioXformBuilderExMovementMethodType
¶ Bases:
object
Represents the Xform movement type
Enum Members
Enum Member Enum Member Description WCS Translate in principal direction View Translate in view direction Vector Translate in vector direction Plane Translate on a plane Normal Translate in normal direction Polygon Translate in polygon direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-