StudioXformBuilderExAdvancedMethodType Enumeration¶
NXOpen.Features.StudioXformBuilderEx.AdvancedMethodType is an alias for NXOpen.Features.StudioXformBuilderExAdvancedMethodType
-
class
NXOpen.Features.
StudioXformBuilderExAdvancedMethodType
¶ Bases:
object
Represents the advanced method type
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderExAdvancedMethodOptionType
instead.Enum Members
Enum Member Enum Member Description ProportionalMovement Proportional movement Falloff Fall off, it is deprecated in NX85 release KeepContinuity Keep continuity, it is deprecated in NX85 release LockRegion Lock region InsertKnot Insert knot AdvanceOff Turn off advanced methods -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-