StudioXformBuilderAdvancedMethodType Enumeration¶
NXOpen.Features.StudioXformBuilder.AdvancedMethodType is an alias for NXOpen.Features.StudioXformBuilderAdvancedMethodType
-
class
NXOpen.Features.
StudioXformBuilderAdvancedMethodType
¶ Bases:
object
Represents the advanced method type
Enum Members
Enum Member Enum Member Description ChangeDegree Change degree Falloff Fall off ProportionalMovement Proportional movement KeepContinuity Keep continuity LockRegion Lock region InsertKnot Insert knot AdvanceOff Turn off advanced methods -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-