StudioSplineBuilderExWCSOptionType Enumeration¶
NXOpen.Features.StudioSplineBuilderEx.WCSOptionType is an alias for NXOpen.Features.StudioSplineBuilderExWCSOptionType
-
class
NXOpen.Features.
StudioSplineBuilderExWCSOptionType
¶ Bases:
object
WCS principal axis or plane types
Enum Members
Enum Member Enum Member Description X Along X axis Y Along Y axis Z Along Z axis YZ In YZ plane XZ In XZ plane XY In XY plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-