StepBuilderStepWallMethods Enumeration

NXOpen.Features.StepBuilder.StepWallMethods is an alias for NXOpen.Features.StepBuilderStepWallMethods

class NXOpen.Features.StepBuilderStepWallMethods

Bases: object

Represents face operation applied to the step wall face

Enum Members

Enum Member Enum Member Description
Normal Orients the step-wall face normal to the input face
OffsetofStepFace Makes the step-wall face offset from the step face
RuledRamp Replaces the step-wall face with a ruled ramp face
VariableOffsetRamp Replaces the step-wall face with a variable offset ramp face
Blend Blends the step-wall face
ExtendtoNext Extends the wall face to intersect the next face
ExtendtoSelected Extends the wall face to a selected face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.