StepBuilderStepNewTypes Enumeration¶
NXOpen.Features.StepBuilder.StepNewTypes is an alias for NXOpen.Features.StepBuilderStepNewTypes
-
class
NXOpen.Features.
StepBuilderStepNewTypes
¶ Bases:
object
Represents the step feature new type since NX12
Enum Members
Enum Member Enum Member Description Thick Adds a step to thick a face. Thin Adds a step to thin a face. Jog Adds a step to thin a belt face and wall face. Chamfer Adds a step at the edge of a face similar to a chamfer -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-