StepBuilderStepFaceMethods Enumeration¶
NXOpen.Features.StepBuilder.StepFaceMethods is an alias for NXOpen.Features.StepBuilderStepFaceMethods
-
class
NXOpen.Features.
StepBuilderStepFaceMethods
¶ Bases:
object
Represents face operations applied to the step face
Enum Members
Enum Member Enum Member Description Normal Orients the step face normal to the stationary face AlignwithReferenceFace Aligns the step face with the reference face RuledRamp Replaces the step face with a ruled ramp face VariableOffsetRamp Replaces the step face with a variable offset ramp face Blend Blends the step face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-