StepBuilderDepthMethods Enumeration

NXOpen.Features.StepBuilder.DepthMethods is an alias for NXOpen.Features.StepBuilderDepthMethods

class NXOpen.Features.StepBuilderDepthMethods

Bases: object

Represents face operations applied to the motion face

Enum Members

Enum Member Enum Member Description
OffsetFace Offsets the motion face to produce a step
ToSelected Replaces the motion face with a selected face to produce a step
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.