SpineCurveBuilderArcSegmentsTypes Enumeration

NXOpen.Features.SpineCurveBuilder.ArcSegmentsTypes is an alias for NXOpen.Features.SpineCurveBuilderArcSegmentsTypes

class NXOpen.Features.SpineCurveBuilderArcSegmentsTypes

Bases: object

This enum represents the arc segments types

Enum Members

Enum Member Enum Member Description
Simple
Smooth
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.