SmoothCurveStringBuilderTypes Enumeration

NXOpen.Features.SmoothCurveStringBuilder.Types is an alias for NXOpen.Features.SmoothCurveStringBuilderTypes

class NXOpen.Features.SmoothCurveStringBuilderTypes

Bases: object

the type of input curves.

Enum Members

Enum Member Enum Member Description
FreeCurves
CurvesOnSurfaces
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.