SilhouetteFlangeBuilderReferenceDirectionOptions Enumeration¶
NXOpen.Features.SilhouetteFlangeBuilder.ReferenceDirectionOptions is an alias for NXOpen.Features.SilhouetteFlangeBuilderReferenceDirectionOptions
-
class
NXOpen.Features.
SilhouetteFlangeBuilderReferenceDirectionOptions
¶ Bases:
object
Reference direction options
Enum Members
Enum Member Enum Member Description FaceNormal Create flange along face normal Vector Create flange along reference vector NormalDraft Create flange along silhouette curve and face normal VectorDraft Create flange along silhouette curve and reference vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-