SilhouetteFlangeBuilderOutputSurfaceOptions Enumeration¶
NXOpen.Features.SilhouetteFlangeBuilder.OutputSurfaceOptions is an alias for NXOpen.Features.SilhouetteFlangeBuilderOutputSurfaceOptions
-
class
NXOpen.Features.
SilhouetteFlangeBuilderOutputSurfaceOptions
¶ Bases:
object
Output surface options
Enum Members
Enum Member Enum Member Description BlendFlange Output blend and flange surfaces PipeOnly Output pipe FlangeOnly Output flange surface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-