AddDataSetBuilder Class |
This class is used to add a dataset to an item in Teamcenter |
AlongGuideCut Class |
Represents a corner cut feature |
AlongGuideCutBuilder Class |
Represents a NXOpen.Features.ShipDesign.AlongGuideCut builder |
AnchorPoint Class |
Represents a NXOpen.Features.ShipDesign.AnchorPoint builder. |
AnchorPointList Class |
Represents a list of objects. |
Bracket Class |
Represents a bracket feature.
|
BracketBuilder Class |
|
BuiltUpBlockBuilder Class |
Represents a NXOpen.Features.ShipDesign.BuiltUpBlockBuilder |
BuiltUpManModeBuilder Class |
This class allows you to set the NX Ship BuiltUp Profile Manufacturing Mode for one or more components. |
BuiltUpOffsetBuilder Class |
Represents a NXOpen.Features.ShipDesign.BuiltUpOffsetBuilder . |
BulkHeadListItemBuilder Class |
Represents a NXOpen.Features.ShipDesign.BulkHeadListItemBuilder |
BulkHeadListItemBuilderList Class |
Represents a list of objects. |
BulkHeads Class |
Represents a bulk head feature |
BulkHeadsBuilder Class |
Represents a NXOpen.Features.ShipDesign.BulkHeads builder |
CollarPlate Class |
Represents a collar plate feature.
|
CollarPlateBuilder Class |
|
CompareModeBuilder Class |
This class is used to compare between the two Shipbuilding modes of Design and Manufacturing. |
ConceptFromSpreadsheet Class |
Represents a concept from spreadsheet feature |
ConceptFromSpreadsheetBuilder Class |
Represents a NXOpen.Features.ShipDesign.ConceptFromSpreadsheet builder |
CopyObjectsBuilder Class |
Represents a NXOpen.Features.ShipDesign.CopyObjectsBuilder It is used in Ship Building Application. |
CopyPasteNewBuilder Class |
Represents a NXOpen.Features.ShipDesign.CopyPasteNewBuilder It is used in Ship Building Application. |
CornerCut Class |
Represents a corner cut feature |
CornerCutBuilder Class |
Builder used to create or edit a NXOpen.Features.ShipDesign.CornerCut feature. |
CornerCutListItemBuilder Class |
Used to supply the list of corner cut locations and seam curves to the NXOpen.Features.ShipDesign.CornerCutBuilder |
CornerCutListItemBuilderList Class |
Represents a list of objects. |
CustomBracket Class |
Represents a custom bracket feature |
CustomBracketBuilder Class |
Represents a NXOpen.Features.ShipDesign.CustomBracket builder |
Cutout2 Class |
Represents a cutout2 feature |
Cutout2Builder Class |
Represents a NXOpen.Features.ShipDesign.Cutout2 builder |
CuttingSideFacesBuilder Class |
Used to create a NXOpen.Features.ShipDesign.CuttingSideFacesBuilder which is used to attribute the cutting side, and opposing cutting side, faces on the plate bodies. |
Deck Class |
Represents a Deck feature in Basic Design. |
DeckBuilder Class |
This class is used to create or edit a NXOpen.Features.ShipDesign.Deck feature. |
DeckListBuilder Class |
This builder allows you to define the general arrangement view information. |
DeckListItemBuilder Class |
Represents a DeckListItemBuilder. |
DeckListItemBuilderList Class |
Represents a list of objects. |
Decks Class |
Represents a decks feature |
DecksBuilder Class |
Represents a NXOpen.Features.ShipDesign.Decks builder. |
DeleteSeamBuilder Class |
Used to create a NXOpen.Features.ShipDesign.DeleteSeamBuilder which is used to delete the seams from the ship structural components. |
DisplaySolidBuilder Class |
This class is used to identify ship structure that is to have a temporary solid display built for it. |
Divide Class |
Represents divide feature(s) |
DivideBuilder Class |
Represents a Features.ShipDesign.Divide builder which is used to edit all divide features. |
DrawingAnnotationBuilder Class |
This builder allows you to define the drawing annotation information. |
DrawingPartBuilder Class |
Represents a NXOpen.Features.ShipDesign.DrawingPartBuilder . |
DrawingPartBuilderList Class |
Represents a list of objects. |
DrawingSheetBuilder Class |
Represents a NXOpen.Features.ShipDesign.DrawingSheetBuilder . |
DrawingSheetBuilderList Class |
Represents a list of objects. |
DrawingTemplateBuilder Class |
Represents a drawing template selection block |
DvToMvMapping Class |
Represents a plate feature |
DvToMvMappingBuilder Class |
Represents a NXOpen.Features.ShipDesign.DvToMvMapping builder. |
EdgeCut Class |
Represents a edge cut feature |
EdgeCutBuilder Class |
Represents a NXOpen.Features.ShipDesign.EdgeCut builder. |
EdgeReinforcement Class |
Represents a edge reinforcement feature. |
EdgeReinforcementBuilder Class |
Represents a NXOpen.Features.ShipDesign.EdgeReinforcement builder which is used to create or edit a edge reinforcement system feature. |
EditBoundaryBuilder Class |
Used to create a NXOpen.Features.ShipDesign.EditBoundaryBuilder which is used to change the boundaries and split knuckle locations of profile systems. |
EditContextAttributesBuilder Class |
Represents the class Features. |
EditStockBuilder Class |
Used to create a NXOpen.Features.ShipDesign.EditStockBuilder which is used to change the stock information on the basic design features. |
EditWeldingBuilder Class |
Used to create a NXOpen.Features.ShipDesign.EditWeldingBuilder which is used to change the welding characteristics on the seams in the plate systems. |
EndCut Class |
Represents an end cut feature |
EndCutBuilder Class |
Represents a NXOpen.Features.ShipDesign.EndCut builder. |
ExamineSteelFeatureBuilder Class |
Represents the examine steel feature builder to examine steel feature. |
ExcessMaterial Class |
Represents a excess material feature |
ExcessMaterialBuilder Class |
Represents a NXOpen.Features.ShipDesign.ExcessMaterial builder. |
ExpansionDrawing Class |
Represents a expansion drawing feature. |
ExpansionDrawingBuilder Class |
Represents a NXOpen.Features.ShipDesign.ExpansionDrawingBuilder . |
FeatureParmsBuilder Class |
This class is used to create or edit the information shared among all Ship Design features. |
FeaturesBatchOperationBuilder Class |
Use this to cycle through the assembly components and perform the operation globally on the specified feature type. |
FeaturesToTagBuilder Class |
This class is used to add an attribute to profile features that have been modified by the user to display a ‘Metal to Metal’ design ‘feature’. |
FilterBuilder Class |
A builder that allows the user to define common properties of ship objects and then add objects of similar properties to the select object list. |
FrameBarOut Class |
Represents a FrameBarOut |
FrameBarOutBuilder Class |
Represents a NXOpen.Features.ShipDesign.FrameBarOut builder. |
GeneralArrangementViewBuilder Class |
This builder allows you to define the general arrangement view information. |
GenericPlateSystem Class |
Represents a Generic Plate System feature. |
GenericPlateSystemBuilder Class |
This class is used to create or edit a NXOpen.Features.ShipDesign.GenericPlateSystem feature. |
Hull Class |
Represents a Hull feature. |
HullBuilder Class |
This class is used to create or edit a NXOpen.Features.ShipDesign.Hull feature. |
InsertFramesBuilder Class |
Represents a NXOpen.Features.ShipDesign.InsertFramesBuilder builder |
InsertSheetBody Class |
Represents a insert sheet body feature |
InsertSheetBodyBuilder Class |
Represents a NXOpen.Features.ShipDesign.InsertSheetBody builder |
InteractiveAnnotationBuilder Class |
Represents a NXOpen.Features.ShipDesign.InteractiveAnnotationBuilder builder . |
InverseBendingLines Class |
Represents a inverse bending lines feature |
InverseBendingLinesBuilder Class |
Used to create or edit a NXOpen.Features.ShipDesign.InverseBendingLines feature. |
ItFrameListItemBuilder Class |
Represents a NXOpen.Features.ShipDesign.ItFrameListItemBuilder |
ItFrameListItemBuilderList Class |
Represents a list of objects. |
ItFrames Class |
Represents a Inter Transverse Frame feature |
ItFramesBuilder Class |
Represents a NXOpen.Features.ShipDesign.ItFrames builder |
KnuckledProfiles Class |
Represents a knuckled profiles manufacturing preparation feature |
KnuckledProfilesBuilder Class |
Represents a NXOpen.Features.ShipDesign.KnuckledProfiles builder |
LabellingRoomsBuilder Class |
Represents a Features.ShipDesign.LabellingRoomsBuilder builder |
LongitudinalBulkhead Class |
Represents a Longitudinal Bulkhead feature. |
LongitudinalBulkheadBuilder Class |
This class is used to create or edit a NXOpen.Features.ShipDesign.LongitudinalBulkhead feature. |
MainDimensions Class |
Represents a main dimensions feature |
MainDimensionsBuilder Class |
Represents a NXOpen.Features.ShipDesign.MainDimensions builder. |
ManufacturingAssemblyNavigatorBuilder Class |
This class is used to define Manufacturing Assembly Structure. |
ManufacturingDataBuilder Class |
This class is used to generate Manufacturing data. |
ManufacturingOut Class |
Represents a ManufacturingOut |
ManufacturingOutBuilder Class |
Represents a NXOpen.Features.ShipDesign.ManufacturingOut builder |
ManufacturingPreparation Class |
Represents a manufacturing preparation feature |
ManufacturingPreparationBuilder Class |
This builder is used to adds attributes to the part and body identifying manufacturing related data. |
ManufacturingStockBuilder Class |
Represents a NXOpen.Features.ShipDesign.ManufacturingStockBuilder builder. |
MarkingLine Class |
Represents a marking line feature. |
MarkingLineBuilder Class |
Represents a MarkingLine Feature builder |
MarkingLineDesign Class |
Represents a marking line feature. |
MarkingLineDesignBuilder Class |
Represents a new MarkingLine Feature builder. |
MaterialAllowanceBuilder Class |
Represents the material allowance feature builder to examine steel feature. |
MaterialEstimationBuilder Class |
Represents the class Features. |
MirrorShipStructureBuilder Class |
Copy the selected parts (components) about the Mirror Plane with full model history and feature data. |
MoveToContainerBuilder Class |
This class is used to move detail design parts to a new ship container. |
OrientationAngleMethodsBuilder Class |
This class defines the method of angle definition used in the definition of the region’s orientation. |
OrientationDefinition Class |
Represents a Orientation SubObject. |
OrientationDefinitionBuilder Class |
This class defines the top level object for use in definining the orientation of stiffeners and edge reinforcements. |
OrientationPointMethodsBuilder Class |
This class is used to define the boundary of the regions when definining the orientation of a profile. |
OrientationRegionItemBuilder Class |
This class defines each region of the orientation. |
OrientationRegionItemBuilderList Class |
Represents a list of objects. |
PenetrationAssociationBuilder Class |
Represents a NXOpen.Features.ShipDesign.PenetrationAssociationBuilder builder |
PenetrationAttachment Class |
Represents the Penetration Attachment object. |
PenetrationCutoutBuilder Class |
Represents a NXOpen.Features.ShipDesign.PenetrationRequest builder |
PenetrationFolder Class |
Represents the Penetration Folder object. |
PenetrationList Class |
Represents the Penetration List object. |
PenetrationManager Class |
Contains the collection objects for creating and iterating over Penetration Request Properties objects. |
PenetrationRequest Class |
Represents the Penetration Request object. |
PenetrationRequestBuilder Class |
Represents a NXOpen.Features.ShipDesign.PenetrationRequest builder |
PenetrationRequestCollection Class |
Represents a NXOpen.Mechatronics.FunctionObjectCollection |
PenetrationRequestForCutoutBuilder Class |
Represents a Features.ShipDesign.PenetrationRequest builder |
PenetrationReviewRequestBuilder Class |
Represents a Features.ShipDesign.PenetrationRequest builder |
PenetrationSite Class |
Represents the Penetration Site object. |
PenetrationUtils Class |
Contains various penetration utility methods |
Pillar Class |
Represents a Pillar feature |
PillarBuilder Class |
Represents a NXOpen.Features.ShipDesign.Pillar builder |
PillarSystem Class |
Represents a pillar system feature. |
PillarSystemBuilder Class |
Represents a NXOpen.Features.ShipDesign.PillarSystem builder which is used to create or edit a pillar system feature. |
PinJig Class |
Represents a Pinjig feature |
PinJigBuilder Class |
Represents a NXOpen.Features.ShipDesign.PinJig builder |
PlaneListBuilder Class |
This class is used to place a plane into a list. |
PlaneListBuilderList Class |
Represents a list of objects. |
PlanePairBuilder Class |
This class is used to define a pair of planes in a list. |
Plate Class |
Represents a plate feature |
PlateBoundaryOptionBuilder Class |
|
PlateBoundaryOptionBuilderList Class |
Represents a list of objects. |
PlateBuilder Class |
Represents a NXOpen.Features.ShipDesign.Plate builder. |
PlateChamfer Class |
Represents a plate chamfer feature |
PlateChamferBuilder Class |
Represents a NXOpen.Features.ShipDesign.PlateChamfer builder. |
PlateDivide Class |
Represents a plate divide feature |
PlateDivideBuilder Class |
Represents a Features.ShipDesign.PlateDivide builder which is used to edit a plate divide feature. |
PlatePreparation Class |
Represents a ship plate preparation feature |
PlatePreparationBuilder Class |
Used to create or edit a NXOpen.Features.ShipDesign.PlatePreparation feature. |
PlateStockBuilder Class |
This builder allows you to define the stock information for plate system features in ship design. |
PlateSystem Class |
Represents a Plate System feature. |
PlateSystemBuilder Class |
This class is used to create or edit the information shared between all the Basic Design plate system features in the Ship Design application. |
PointPairBuilder Class |
This class is used to define a pair of points in a list. |
Profile Class |
Represents a profile feature |
ProfileBuilder Class |
Represents a NXOpen.Features.ShipDesign.Profile builder |
ProfileCutout Class |
Represents a profile cutout feature for NX8. |
ProfileCutoutBuilder Class |
Represents a NXOpen.Features.ShipDesign.ProfileCutout builder |
ProfileList Class |
Represents a profile list feature |
ProfileListBuilder Class |
Represents a NXOpen.Features.ShipDesign.ProfileList builder |
ProfileSystem Class |
Represents a profile system feature. |
ProfileSystemBuilder Class |
This class is used to create or edit the information shared between all the Basic Design profile system features in the Ship Design application. |
ProfileTransition Class |
Represents a profile transition feature |
ProfileTransitionBuilder Class |
Builder used to create or edit a NXOpen.Features.ShipDesign.ProfileTransition feature. |
ProjectSetupBuilder Class |
Represents a project setup builder for ship.
|
QualifySketchBuilder Class |
Represents a NXOpen.Features.ShipDesign.QualifySketchBuilder builder. |
ReadDataSetBuilder Class |
This class will read a data set file from Team Center |
RebaseBuilder Class |
This class is used to synchronize the end cuts from the ones in mfg group to design group. |
ReferenceLine Class |
Represents a reference line feature. |
ReferenceLineBuilder Class |
Represents a NXOpen.Features.ShipDesign.ReferenceLine builder. |
RemoveSplitBuilder Class |
Represents a NXOpen.Features.ShipDesign.RemoveSplitBuilder . |
ReverseSplitBuilder Class |
This class is used to provide the capability to reverse the split interaction between ship structures. |
RollingLine Class |
Represents a rolling line feature. |
RollingLineBuilder Class |
Represents a NXOpen.Features.ShipDesign.RollingLine builder. |
RoomAttributeListBuilder Class |
The builder to define room attributes |
RoomAttributesBuilder Class |
Represents a NXOpen.Features.ShipDesign.RoomAttributesBuilder It is used in Ship General Arrangement Application. |
RoomBuilder Class |
Represents a room builder for general arrangement.
|
RoomContainerBuilder Class |
Represents a Features.ShipDesign.RoomContainerBuilder builder |
RoomPanelBuilder Class |
Represents a Features.ShipDesign.RoomPanelBuilder builder |
Seam Class |
Represents a ship design seam feature. |
SeamBlockBuilder Class |
Represents a NXOpen.Features.ShipDesign.SeamBlockBuilder |
SeamBlockBuilderList Class |
Represents a list of objects. |
SeamBuilder Class |
A NXOpen.Features.ShipDesign.SeamBuilder used to create or edit a ship design NXOpen.Features.ShipDesign.Seam feature. |
SectionDrawingBuilder Class |
This builder allows you to define the section drawing information. |
SectionEditorBuilder Class |
Represents a NXOpen.Features.ShipDesign.SectionEditorBuilder builder. |
SectionViewBuilder Class |
It represents NXOpen.Features.ShipDesign.SectionViewBuilder . |
SectionViewBuilderList Class |
Represents a list of objects. |
SelectPartBuilder Class |
Represents a NXOpen.Features.ShipDesign.SelectPartBuilder . |
SelectStructuresBuilder Class |
This builder allows you to select structures in NXOpen.Features.ShipDesign.GeneralArrangementViewBuilder . |
SetModeBuilder Class |
This class is used to set the mode to design or manufacturing. |
ShellExpansion Class |
Represents a shell expansion feature |
ShellExpansionBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShellExpansion builder |
ShellTemplate Class |
Represents a shell template feature. |
ShellTemplateBuilder Class |
Used to edit or create a NXOpen.Features.ShipDesign.ShellTemplate feature. |
ShipAttributeHolder Class |
Represents a NXOpen.Features.ShipDesign.ShipAttributeHolder builder |
ShipContainerBuilder Class |
This class is used to specify the container part for the Ship Structures application, i. |
ShipCoordinates Class |
Represents a ship coordinates feature |
ShipCoordinatesBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipCoordinates builder |
ShipCutout Class |
Represents a ship cutout feature |
ShipCutoutBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipCutout builder |
ShipDesignPreferencesBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilder which is used to change default object display settings for ship structures. |
ShipDesignVersionUpBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipDesignVersionUpBuilder builder. |
ShipEndCut Class |
Represents a ship end cut feature |
ShipEndCutBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipEndCut builder |
ShipFeatureConverter Class |
This class is used to convert/upgrade legacy Ship Design features. |
ShipFlatPattern Class |
Represents a ship flat pattern feature |
ShipFlatPatternBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipFlatPattern builder |
ShipIntersections Class |
Represents a ship intersection feature |
ShipIntersectionsBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipIntersections builder |
ShipNameFieldBuilder Class |
A field, combined with other fields, to generate a name for a Ship Basic Design Object such as a Deck. |
ShipNamesBuilder Class |
This class provides the mechanism for defining the names of Basic Design objects such as Decks, Bulkheads, Stiffener Systems, etc. |
ShipNamesBuilderList Class |
Represents a list of objects. |
ShipNamesListBuilder Class |
This class provides a list of :py:class:`NXOpen.Features.ShipDesign.ShipNamesBuilder`objects. |
ShipPreparationBuilder Class |
Creates a builder used to prepare basic design data for meshing. |
ShipPreparationInfo Class |
Used to interrogate and change the processing within the NXOpen.Features.ShipDesign.ShipPreparationBuilder . |
ShipProfileCutout Class |
Represents a profile cutout feature for NX75 using sketch expression modifier block. |
ShipProfileCutoutBuilder Class |
Represents a NXOpen.Features.ShipDesign.ProfileCutout builder for editing legacy(NX75) profile cutout feature. |
ShipSection Class |
Represents a ship section feature |
ShipSectionBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipSection builder |
ShipStructureBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipStructureBuilder . |
ShipTrimBody Class |
Represents a ship trim body feature |
ShipTrimBodyBuilder Class |
Represents a NXOpen.Features.ShipDesign.ShipTrimBodyBuilder . |
SmartRule Class |
Represents a smart rule feature. |
SmartRuleBuilder Class |
Represents a NXOpen.Features.ShipDesign.SmartRule builder |
SplitProfilePlateBuilder Class |
Represents a NXOpen.Features.ShipDesign.SplitProfilePlateBuilder . |
SplitStandardPart Class |
Represents a split standard part feature. |
SplitStandardPartBuilder Class |
Represents a NXOpen.Features.ShipDesign.SplitStandardPartBuilder . |
StandardPart Class |
Represents a standard part feature. |
StandardPartFrameworkBuilder Class |
Represents the standard part framework builder to add or edit ship standard part. |
StandardPartItemBuilder Class |
Represents the ship standard part item builder. |
StandardPartItemBuilderList Class |
Represents a list of objects. |
StandardPartSCAssist Class |
Represents |
SteelCollarPlate Class |
Represents a collar plate steel feature |
SteelCollarPlateBuilder Class |
Represents a NXOpen.Features.ShipDesign.SteelCollarPlate builder |
SteelDistribution Class |
Represents a steel distribution feature |
SteelDistributionBuilder Class |
Represents a NXOpen.Features.ShipDesign.SteelDistribution builder |
SteelFeatureSpreadsheetBuilder Class |
Represents a NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder builder. |
SteelInsulation Class |
Represents a steel insulation feature. |
SteelInsulationBoundaryBuilder Class |
Represents a Steel Insulation Boundary builder. |
SteelInsulationBoundaryBuilderList Class |
Represents a list of objects. |
SteelInsulationBuilder Class |
Represents a builder that is used to create or edit a NXOpen.Features.ShipDesign.SteelInsulation feature. |
SteelSupport Class |
Represents a steel support feature |
SteelSupportBuilder Class |
Represents a NXOpen.Features.ShipDesign.SteelSupport builder |
SteelVentHoles Class |
Represents a ship vent holes feature |
SteelVentHolesBuilder Class |
Represents a NXOpen.Features.ShipDesign.SteelVentHoles builder |
Stiffener Class |
Represents a stiffener feature |
StiffenerBuilder Class |
Represents a NXOpen.Features.ShipDesign.Stiffener builder |
StiffenerBySupportPathBuilder Class |
This class defines the builder to collect stiffener by support path data for Stiffener feature. |
StiffenerLimitBuilder Class |
This class defines the path limit method used by a Stiffener or Edge Reinforcement feature. |
StiffenerStockBuilder Class |
This class defines the Profile or Plate stock for a Stiffener or Edge Reinforcement feature. |
StiffenerSystem Class |
Represents a stiffener system feature. |
StiffenerSystemBuilder Class |
This class is used to create or edit a NXOpen.Features.ShipDesign.StiffenerSystem feature. |
SubSystemBuilder Class |
This class is used to edit the Sub System Definition of a NXOpen.Features.ShipDesign.SubSystems feature. |
SubSystemBuilderList Class |
Represents a list of objects. |
SubSystems Class |
Represents a sub systems feature. |
SubSystemsBuilder Class |
This class is used to edit a NXOpen.Features.ShipDesign.SubSystems feature. |
SynchronizeDesignViewBuilder Class |
This class is used to synchronize body features from design view to manufacturing view. |
ThicknessDirectionBuilder Class |
This class allows you to define the thickness direction for plate system features in Ship Basic Design and and for grid planes in Ship Concept Design. |
TraceLines Class |
Represents a trace lines feature |
TraceLinesBuilder Class |
Represents a NXOpen.Features.ShipDesign.TraceLines builder |
TransFrame Class |
Represents a TransVerse Frame feature |
TransFrameBuilder Class |
Represents a NXOpen.Features.ShipDesign.TransFrame builder |
TransFrameListItemBuilder Class |
Represents a NXOpen.Features.ShipDesign.TransFrameListItemBuilder |
TransFrameListItemBuilderList Class |
Represents a list of objects. |
TransitionBuilder Class |
This is to create a NXOpen.Features.ShipDesign.TransitionBuilder which is used to create Detail Design elements from Basic Design elements. |
TransverseBulkhead Class |
Represents a Transverse Bulkhead feature. |
TransverseBulkheadBuilder Class |
This class is used to create or edit a NXOpen.Features.ShipDesign.TransverseBulkhead feature. |
UnfoldedMinRecBuilder Class |
Represents the class Features. |
UpdateShipLibrary Class |
Represents a update ship library feature |
UpdateShipLibraryBuilder Class |
Represents a NXOpen.Features.ShipDesign.UpdateShipLibrary builder |
ValidateModelBuilder Class |
This is to create a NXOpen.Features.ShipDesign.ValidateModelBuilder which is used to validate Basic Design Structures. |
VentHolesMarking Class |
Represents a vent holes marking feature |
VentHolesMarkingBuilder Class |
Represents a NXOpen.Features.ShipDesign.VentHolesMarking builder |
VentilationHoles2 Class |
Represents a ventilation holes2 feature |
VentilationHoles2Builder Class |
Represents a NXOpen.Features.ShipDesign.VentilationHoles2 builder |
VerifyPenetrationBuilder Class |
Represents a NXOpen.Features.ShipDesign.VerifyPenetrationBuilder builder |
WeightAndCGBuilder Class |
Represents the class Features. |
WeldCut Class |
Represents a weld cut feature |
WeldCut2 Class |
Represents a weld cut2 feature |
WeldCut2Builder Class |
Represents a NXOpen.Features.ShipDesign.WeldCut2 builder |
WeldCutBuilder Class |
Represents a NXOpen.Features.ShipDesign.WeldCut builder |
YFrameBuilder Class |
Represents a NXOpen.Features.ShipDesign.YFrameBuilder |
ZFrameBuilder Class |
Represents a NXOpen.Features.ShipDesign.ZFrameBuilder |