UpdateShipLibraryBuilderShipLibAssemblyOption Enumeration¶
NXOpen.Features.ShipDesign.UpdateShipLibraryBuilder.ShipLibAssemblyOption is an alias for NXOpen.Features.ShipDesign.UpdateShipLibraryBuilderShipLibAssemblyOption
-
class
NXOpen.Features.ShipDesign.
UpdateShipLibraryBuilderShipLibAssemblyOption
¶ Bases:
object
Assembly update library options
Enum Members
Enum Member Enum Member Description WorkPart update the library in the current work part only WorkPartandComponents update the library in the current work part and all of its components WorkPartandComponentswithLibraries update any parts with existing libraries starting in the current work part and all of its components -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-