TransitionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
TransitionBuilder
¶ Bases:
NXOpen.Builder
This is to create a
NXOpen.Features.ShipDesign.TransitionBuilder
which is used to create Detail Design elements from Basic Design elements.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateTransitionBuilder()
Default values.
Property Value SelectPart.SectionFrameType Section TransitionMethod UpdateExisting TransitionType Section New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
SectionMappingFile | Returns or sets the file name of the section mapping from the native file system |
SelectPart | Returns the ship basic design part |
Tag | Returns the Tag for this object. |
TransitionMethod | Returns or sets the transition method. |
TransitionType | Returns or sets the transition type. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DryRun | Executes a dry run to check whether there are circular references in the basic design structure model and whether the intersection seam is using split or not. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFrameParts | Set frame part names. |
SetSectionBlockParts | The section block part file name. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TransitionBuilderTransitionMethods Enumeration | Transition Method. |
TransitionBuilderTransitionTypes Enumeration | Transition Type. |
Property Detail¶
SectionMappingFile¶
-
TransitionBuilder.
SectionMappingFile
¶ Returns or sets the file name of the section mapping from the native file system
-------------------------------------
Getter Method
Signature
SectionMappingFile
Returns: Return type: str New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionMappingFile
Parameters: filename (str) – New in version NX10.0.3.
License requirements: nx_ship_basic (“Ship Basic Design”)
SelectPart¶
-
TransitionBuilder.
SelectPart
¶ Returns the ship basic design part
-------------------------------------
Getter Method
Signature
SelectPart
Returns: Return type: NXOpen.Features.ShipDesign.SelectPartBuilder
New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
TransitionMethod¶
-
TransitionBuilder.
TransitionMethod
¶ Returns or sets the transition method.
-------------------------------------
Getter Method
Signature
TransitionMethod
Returns: Return type: NXOpen.Features.ShipDesign.TransitionBuilderTransitionMethods
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransitionMethod
Parameters: method ( NXOpen.Features.ShipDesign.TransitionBuilderTransitionMethods
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
TransitionType¶
-
TransitionBuilder.
TransitionType
¶ Returns or sets the transition type.
-------------------------------------
Getter Method
Signature
TransitionType
Returns: Return type: NXOpen.Features.ShipDesign.TransitionBuilderTransitionTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransitionType
Parameters: type ( NXOpen.Features.ShipDesign.TransitionBuilderTransitionTypes
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Method Detail¶
DryRun¶
-
TransitionBuilder.
DryRun
¶ Executes a dry run to check whether there are circular references in the basic design structure model and whether the intersection seam is using split or not.
Signature
DryRun()
New in version NX11.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
SetFrameParts¶
-
TransitionBuilder.
SetFrameParts
¶ Set frame part names.
Signature
SetFrameParts(framePartFilenames)
Parameters: framePartFilenames (list of str) – New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
SetSectionBlockParts¶
-
TransitionBuilder.
SetSectionBlockParts
¶ The section block part file name.
Signature
SetSectionBlockParts(sectionParts)
Parameters: sectionParts (list of str) – New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Validate¶
-
TransitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.