SubSystemsBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.SubSystemsBuilder.Types is an alias for NXOpen.Features.ShipDesign.SubSystemsBuilderTypes
-
class
NXOpen.Features.ShipDesign.
SubSystemsBuilderTypes
¶ Bases:
object
Used to indicate the type of sub system definition that is being edited.
Enum Members
Enum Member Enum Member Description Plate Plate system, any system using plate stock. Profile Profile system, any system using stiffener stock. Pillar Pillar system, any system using spreadsheet defined stock. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-