StiffenerStockBuilderStockSectionType Enumeration¶
NXOpen.Features.ShipDesign.StiffenerStockBuilder.StockSectionType is an alias for NXOpen.Features.ShipDesign.StiffenerStockBuilderStockSectionType
-
class
NXOpen.Features.ShipDesign.
StiffenerStockBuilderStockSectionType
¶ Bases:
object
Type of Stiffener/Edge Reinforcement stock: Profile or Plate
Enum Members
Enum Member Enum Member Description Profile Profile Stock Plate Plate Stock BuiltUp Built Up Stock -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-