StiffenerLimitBuilderLimitType Enumeration¶
NXOpen.Features.ShipDesign.StiffenerLimitBuilder.LimitType is an alias for NXOpen.Features.ShipDesign.StiffenerLimitBuilderLimitType
-
class
NXOpen.Features.ShipDesign.
StiffenerLimitBuilderLimitType
¶ Bases:
object
Path limiting method
Enum Members
Enum Member Enum Member Description Value Trim or extend by a fixed distance value. SquareCut Stiffener will extend into limiting geometry. NeatTrim It will automatically create an End Cut that trim the stiffener to the selected geometry. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-