StandardPartItemBuilderDirection Enumeration¶
NXOpen.Features.ShipDesign.StandardPartItemBuilder.Direction is an alias for NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
-
class
NXOpen.Features.ShipDesign.
StandardPartItemBuilderDirection
¶ Bases:
object
Represents the ship standard part installation direction and thickness direction.
Enum Members
Enum Member Enum Member Description Fore fore Aft aft Up up Down down Port port Starboard starboard In in Out out Center center -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-