SplitProfilePlateBuilderToolOptionType Enumeration¶
NXOpen.Features.ShipDesign.SplitProfilePlateBuilder.ToolOptionType is an alias for NXOpen.Features.ShipDesign.SplitProfilePlateBuilderToolOptionType
-
class
NXOpen.Features.ShipDesign.
SplitProfilePlateBuilderToolOptionType
¶ Bases:
object
Represents trim tool type to trim profile or plate solid body.
Enum Members
Enum Member Enum Member Description Plane Select existing datum or face. NewPlane Create a new datum. Extrude Select curve and direction as extrude. Body Select plate or profile body. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-