ShipnamesBuilderVersion Enumeration

class NXOpen.Features.ShipDesign.ShipnamesBuilderVersion

Bases: object

The version of Ship Object naming rule Enum Members

Enum Member Enum Member Description
Legacy
PositionInformation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.