ShipnamesBuilderType Enumeration¶
-
class
NXOpen.Features.ShipDesign.
ShipnamesBuilderType
¶ Bases:
object
The type of Ship Object for which automatically generated names will be created Enum Members
Enum Member Enum Member Description NotSet Hull Deck LongitudinalBulkhead TransverseBulkhead StiffenerSystem EdgeReinforcementSystem PillarSystem Seam GenericPlateSystem StandardPart CollarPlate Bracket Plate Profile Pillar StandardPartCollarPlate StandardPartBracket Grid Room -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-