ShipnameFieldBuilderType Enumeration¶
-
class
NXOpen.Features.ShipDesign.
ShipnameFieldBuilderType
¶ Bases:
object
Field Type Enum Members
Enum Member Enum Member Description Fixed Field with an unchanging string Option Field whose value can be one of several strings Index Field which will have a number generated Any Field whose value will be a user enterred string PositionInformation Field which is generated from mold face plane indicate part location ContextAttributeMap Field whose value comes from context attribute SectionInformation Field whose value comes from section NotSet Unknown Field Type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-