ShipPreparationInfoTypes Enumeration¶
NXOpen.Features.ShipDesign.ShipPreparationInfo.Types is an alias for NXOpen.Features.ShipDesign.ShipPreparationInfoTypes
-
class
NXOpen.Features.ShipDesign.
ShipPreparationInfoTypes
¶ Bases:
object
Used to specify the type of object represented in the data.
Enum Members
Enum Member Enum Member Description Unknown Type of data not known yet. LinkedBody The data represents a linked body feature. LinkedBodyBracket The data represents a linked body feature for the new Bracket body. LinkedEdges The data represents a composite curve feature extracting edges. LinkedCurves The data represents a linked composite curve feature. LinkedFaces The data represents a linked face feature. PlateDivide The data represents a plate divide feature. StiffenerDivide The data represents a stiffener divide feature. StiffenerBySupportDivide The data represents a stiffener divide feature, for a stiffener by support. EdgeReinforcementDivide The data represents a edge reinforcement divide feature. This feature handles splitting edges when needed. EdgeReinforcementEdges The data represents a edge reinforcement divide feature. This feature handles labelling the edges of the linked body. StandardPartBracketDivide The data represents a standard part bracket divide feature. Pillar The data represents a pillar feature. BracketDivide The data represents a bracket divide feature. UserDefined The data represents a user defined divide feature. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-