ShipDesignPreferencesBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilder.Types is an alias for NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilderTypes
-
class
NXOpen.Features.ShipDesign.
ShipDesignPreferencesBuilderTypes
¶ Bases:
object
This enum represents the ship structure types.
Enum Members
Enum Member Enum Member Description Hull Hull type Deck Deck type TransverseBulkhead Transverse Bulkhead type LongitudinalBulkhead Longitudinal Bulkhead type GenericPlateSystem Generic Plate System type StiffenerSystem Stiffener System type EdgeReinforcementSystem Edge Reinforcement System type PillarSystem Pillar System type ScantlingSeam Scantling Seam type ErectionSeam Erection Seam type StrakingSeam Straking Seam type IntersectionSeam Intersection Seam type Bracket Bracket type CollarPlate Collar Plate type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-