ShellTemplateBuilderMarkingTypes Enumeration¶
NXOpen.Features.ShipDesign.ShellTemplateBuilder.MarkingTypes is an alias for NXOpen.Features.ShipDesign.ShellTemplateBuilderMarkingTypes
-
class
NXOpen.Features.ShipDesign.
ShellTemplateBuilderMarkingTypes
¶ Bases:
object
The option for controlling which marking lines are drawn on the plate
Enum Members
Enum Member Enum Member Description NotSet Do not draw template marking lines on plate. XDirectionOnly Draw X direction template marking lines on plate. YDirectionOnly Draw Y direction template marking lines on plate. XandYDirections Draw X and Y direction template marking lines on plate. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-