ShellTemplateBuilderCornerCutTypes Enumeration¶
NXOpen.Features.ShipDesign.ShellTemplateBuilder.CornerCutTypes is an alias for NXOpen.Features.ShipDesign.ShellTemplateBuilderCornerCutTypes
-
class
NXOpen.Features.ShipDesign.
ShellTemplateBuilderCornerCutTypes
¶ Bases:
object
The option for creating corner cuts on the templates.
Enum Members
Enum Member Enum Member Description NotSet Do not add corner cuts. Start Add corner cuts on the start side of each template. End Add corner cuts on the end side of each template. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-