SeamBuilderDefinitionMethods Enumeration¶
NXOpen.Features.ShipDesign.SeamBuilder.DefinitionMethods is an alias for NXOpen.Features.ShipDesign.SeamBuilderDefinitionMethods
-
class
NXOpen.Features.ShipDesign.
SeamBuilderDefinitionMethods
¶ Bases:
object
Used to indicate the method being used to define the seam locations. Not valid for
NXOpen.Features.ShipDesign.SeamBuilderTypes.Intersection
.Enum Members
Enum Member Enum Member Description CurvesPlanesShip Can use curves, planes or other ship structure to define the seam location. The intersection or projection of the selected data with the ship structure defines the seam location. EquallySpaced Create a specified number of seams equidistant between two selected curves. Rectangular Create a rectangular pattern of seams based on an origin, direction, and size of rectangles. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-