SeamBlockBuilderSeamType Enumeration¶
NXOpen.Features.ShipDesign.SeamBlockBuilder.SeamType is an alias for NXOpen.Features.ShipDesign.SeamBlockBuilderSeamType
-
class
NXOpen.Features.ShipDesign.
SeamBlockBuilderSeamType
¶ Bases:
object
this specifies seam type option
Enum Members
Enum Member Enum Member Description FlangeOnly Split the built up flange WebOnly Split the built up web NoFlange Remove the flange -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-