RebaseBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
RebaseBuilder
¶ Bases:
NXOpen.Builder
This class is used to synchronize the end cuts from the ones in mfg group to design group.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateRebaseBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DesignElementToRebase | Returns the selected design elements to rebase. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Rebase | Loops through all the parts and rebases the manufacturing end cut parameters to the values of the corresponding design end cut |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DesignElementToRebase¶
-
RebaseBuilder.
DesignElementToRebase
¶ Returns the selected design elements to rebase.
-------------------------------------
Getter Method
Signature
DesignElementToRebase
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Rebase¶
-
RebaseBuilder.
Rebase
¶ Loops through all the parts and rebases the manufacturing end cut parameters to the values of the corresponding design end cut
Signature
Rebase()
Returns: Return type: int New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
RebaseBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.